By setting a trace event, it is possible to collect only a history of execution in a given section as trace data during program execution process.
This trace event consists of a trace start event and a trace end event.
To use this function, follow the procedure described below.
2.13.3.1 Setting a trace start event and a trace end event
2.13.3.2 Combining multiple events [E1] [E20] [EZ Emulator]
2.13.3.3 Executing the program
2.13.3.4 Editing trace start and trace end events
2.13.3.5 Deleting a trace start or trace end event
Also see "2.17.7 Points to note regarding event setting" for details on trace settings, including the allowable number of valid events. |