Column Chooser dialog box


This dialog box allows you to choose whether or not to display the item listed in this dialog box in the device pin list, and add columns to or delete columns from the device pin list.

Figure A.13

Column Chooser Dialog Box

 

The following items are explained here.

[How to open]

-

In the [Pin Number] tab of the Device Pin List panel, click the button.

-

In the [Macro] tab of the Device Pin List panel, click the button.

-

In the [External Peripheral] tab of the Device Pin List panel, click the button.

[Description of each area]

(1)

Operational object selection area

This area allows you to select the device pin list to be configured in this dialog box.

Pin Number

Configures the device pin list corresponding to the [Pin Number] tab.

Macro

Configures the device pin list belonging to the first layer of the [Macro] tab.

Macro - Pin

Configures the device pin list belonging to the second layer of the [Macro] tab.

External Peripheral

Configures the device pin list belonging to the first layer of the [External Peripheral] tab.

External Peripheral - Pin

Configures the device pin list belonging to the second layer of the [External Peripheral] tab.

 

(2)

Displayed item selection area

Select whether or not to display the item selected in the Operational object selection area in the device pin list.

Checked

Displays the selected item in the device pin list.

Not checked

Hides the selected item in the device pin list.

[Function buttons]

New Column...

Opens the New Column dialog box for adding columns to the device pin list.

Delete Column

Deletes the selected columns from the device pin list.

You can only delete the column which you added using the New Column dialog box.

Default

Restores the column order to the default settings.

Close

Closes this dialog box.