Project Tree panel


This panel displays components of the project (microcontroller, design tool, build tool, etc.) in a tree structure.

Figure A.2

Project Tree Panel

 

The following items are explained here.

[How to open]

-

From the [View] menu, select [Project Tree].

[Description of each area]

(1)

Project tree area

This area displays components of the project (microcontroller, design tool, build tool, etc.) in a tree structure.

(a)

Pin Configurator (Design Tool)

This node consists of the following pin nodes.

Device Pin List

Opens the Device Pin List panel for entering information on the pins of the microcontroller.

Device Top View

Opens the Device Top View panel that displays the information entered in the Device Pin List panel.

[Context menu]

Return to Reset Value

The default settings of the selected node are restored.

Property

Opens the Property panel corresponding to the selected node.