|
|
|
|
fileName
|
Specify the full path of a new project file.
If no file extension is specified, the filename is automatically supplemented.
If the project to be created is a main project (subProject = False) or a subproject (subProject = True), the name is supplemented by ".mtpj" or ".mtsp", respectively.
When the extension is other than that specified, it is replaced by the actual extension.
|
|
micomType
|
Specify the microcontroller type of a new project.
The types that can be specified are shown below.
|
|
|
|
|
MicomType.RH850
|
Project for RH850
|
|
MicomType.RX
|
Project for RX
|
|
MicomType.V850
|
Project for V850
|
|
MicomType.RL78
|
Project for RL78
|
|
MicomType.K0R
|
Project for 78K0R
|
|
MicomType.K0
|
Project for 78K0
|
|
deviceName
|
Specify the device name of the microcontroller of a new project by a string.
|
|
projectKind
|
Specify the type of a new project.
The types that can be specified are shown below.
The following is automatically specified if the microcontroller type is RH850 and "ProjectKind.Auto" is specified or projectKind is not specified.
When the microcontroller is single core: ProjectKind.Application
When the microcontroller is multi-core and main project: ProjectKind.MulticoreBootLoader
When the microcontroller is multi-core and subproject: ProjectKind.MulticoreApplication
|
|
|
|
|
ProjectKind.Application
|
Project for application
|
|
ProjectKind.Library
|
Project for library
|
|
ProjectKind.DebugOnly
|
Debug-dedicated project
|
|
ProjectKind.Empty
|
Project for empty application
|
|
ProjectKind.CppApplication
|
Project for C++ application
|
|
ProjectKind.GHSCCProject
|
CS+ project using an existing GHS project file
|
|
ProjectKind.RI600V4
|
Project for RI600V4
|
|
ProjectKind.RI600PX
|
Project for RI600PX
|
|
ProjectKind.RI850V4
|
Project for RI850V4
|
|
ProjectKind.RI850MP
|
Project for RI850MP
|
|
ProjectKind.RI78V4
|
Project for RI78V4
|
|
ProjectKind.MulticoreBootLoader
|
Project for boot loader for multi-core
|
|
ProjectKind.MulticoreApplication
|
Project for application for multi-core
|
|
ProjectKind.Auto
|
The type of a project is selected in accord with the specification for micomType, deviceName, and subProject (default).
|
|
compiler
|
Specify the compiler to be used.
If the compiler is not specified, it is selected automatically depending on the microcontroller type.
|
|
|
|
|
Compiler.Auto
|
The compiler to be used is selected in accord with the specification for micomType (default).
|
|
Compiler.CC_RH
|
CC-RH
If this argument is not specified when micomType is set to "MicomType.RH850", CC-RH is selected automatically.
|
|
Compiler.CC_RX
|
CC-RX
If this argument is not specified when micomType is set to "MicomType.RX", CC-RX is selected automatically.
|
|
Compiler.CA850
|
CA850
If this argument is not specified when micomType is set to "MicomType.V850" and deviceName is set to "V850E" or "V850ES", CA850 is selected automatically.
|
|
Compiler.CX
|
CX
If this argument is not specified when micomType is set to "MicomType.V850" and deviceName is set to "V850E2", CX is selected automatically.
|
|
Compiler.CC_RL
|
CC-RL
If this argument is not specified when "MicomType.RL78" in CS+ for CC, CC-RL is selected automatically.
|
|
Compiler.CA78K0R
|
CA78K0R
If this argument is not specified when micomType is set to "MicomType.K0R" or "MicomType.RL78" in CS+ for CACX, CA78K0R is selected automatically.
|
|
Compiler.CA78K0
|
CA78K0
If this argument is not specified when micomType is set to "MicomType.K0", CA78K0 is selected automatically.
|
|
Compiler.GHSCC
|
GHSCC
The compiler from Green Hills Software.
|
|
subProject
|
Specify whether to create a main project or a subproject.
False: Create a main project (default).
True: Create a subproject.
|