project.File.Exists


This function confirms whether the file exists in the active project.

[Specification format]

project.File.Exists(fileName)

[Argument(s)]

Argument

Description

fileName

Specify the full path of the file whose existence in the active project is to be checked.

[Return value]

If the specified file existed in the active project: True

If the specified file did not exist in the active project: False

[Detailed description]

-

This function confirms whether the file specified in fileName exists in the active project.

[Example of use]

>>>project.File.Exists("C:/project/sample/src/test.c")
True
>>>