project.File.Information


This function displays the list of the files registered in the active project.

[Specification format]

project.File.Information()

[Argument(s)]

None

[Return value]

List of the files registered in the active project (in a full path)

[Detailed description]

-

This function displays the list of the full path of the files registered in the active project.

[Example of use]

>>>project.File.Information()
C:\prj\src\file1.c
C:\prj\src\file2.c
C:\prj\src\file3.c
>>>