project.Information


This function displays the list of project files.

[Specification format]

project.Information()

[Argument(s)]

None

[Return value]

List of project file names

[Detailed description]

-

This function displays the list of project files of the main project and subprojects included in the loaded project.

[Example of use]

>>>project.Information()
C:\project\sample\test.mtpj
C:\project\sample\sub1\sub1project.mtsp
C:\project\sample\sub2\sub2project.mtsp
>>>