build.Clean


This function runs a clean.

[Specification format]

build.Clean(all = False)

[Argument(s)]

Argument

Description

all

Specify whether to clean a project including subprojects.

True: Clean all project including subprojects.

False: Clean an active project (default).

[Return value]

If a clean was completed successfully: True

If there was an error when running a clean: False

[Detailed description]

-

This function runs a clean of a project (removes the files generated by a build).

-

If all is set to "True", then a clean of the subproject is run.

[Example of use]

>>>build.Clean()
True
>>>