build.Stop


This function stops the currently running build.

[Specification format]

build.Stop()

[Argument(s)]

None

[Return value]

If the build was stopped successfully: True

If there was an error when stopping the build: False

[Detailed description]

-

This function stops the currently running build.

[Example of use]

>>>build.All(True, False)
True
>>>build.Stop()
True
>>>