build.Compile.IncludePath
|
This property sets or refers to the compile options for the active project regarding additional include paths.
[Specification format]
build.Compile.IncludePath = dirlist
|
[Setting(s)]
|
|
dirlist
|
Set the additional include paths as a list of strings.
|
[Reference]
List of additional include paths
[Detailed description]
- | This property sets or refers to the compile options for the active project regarding additional include paths. |
- | Add or change for the referred list to change the setting. |
[Example of use]
>>>incpath1 = build.Compile.IncludePath ... Refer the current setting and add an include path
>>>print incpath1
['include', 'C:\project\inc']
>>>incpath1.append('include2')
>>>build.Compile.IncludePath = incpath1
>>>print build.Compile.IncludePath
['include', 'C:\project\inc', 'include2']
>>>
>>>incpath2 = ['include1', 'include2'] ... Set multiple include paths
>>>build.Compile.IncludePath = incpath2
>>>print build.Compile.IncludePath
['include1', 'include2']
|