This property sets or refers to the setting for output of a ROMized object file, that is, the value of the ROMization process option for the active project. [CA850][CX][CA78K0R]
If the ROMized object file is output: True
If the ROMized object file is not output: False
If the compiler is not supported: None
This property sets or refers to the setting for output of a ROMized object file, that is, the value of the ROMization process option for the active project. |