This property sets or refers to the compile options for the active project regarding defined macros.
[Specification format]
build.Compile.Macro = macrolist
|
[Setting(s)]
|
|
macrolist
|
Set the defined macros as a list of strings.
|
[Reference]
List of defined macros
[Detailed description]
- | This property sets or refers to the compile options for the active project regarding defined macros. |
- | Add or change for the referred list to change the setting. |
[Example of use]
>>>macrolist = build.Compile.Macro ... Refer the current setting and add a defined macro
>>>print macrolist
['RL78']
>>>macrolist.append('78K')
>>>build.Compile.Macro = macrolist
>>>print build.Compile.Macro
['RL78', '78K']
>>>
>>>macrolist = ['macro1', 'macro2'] ... Set multiple defined macros
>>>build.Compile.Macro = macrolist
>>>print build.Compile.Macro
['macro1', 'macro2']
|