build.Link.SectionAlignment


This property sets or refers to the link options for the active project regarding section alignment. [CC-RH][CC-RX][CC-RL]

[Specification format]

build.Link.SectionAlignment = sectionlist

[Setting(s)]

Setting

Description

sectionlist

Set section alignment as a list of strings.

[Reference]

List of section alignment

[Detailed description]

-

This property sets or refers to the link options for the active project regarding section alignment.

-

Add or change for the referred list to change the setting.

[Example of use]

>>>lib1 = build.Link.LibraryFile      ... Refer the current setting and add section alignment
['R_1']
>>>sec1.append('R_2')
>>>build.Link.SectionAlignment = sec1
>>>print build.Link.SectionAlignment
['R_1', 'R_2']
>>>
>>>sec2 = ['R_1', 'R_2']              ... Set multiple section alignment
>>>build.Link.SectionAlignment = sec2
>>>print build.Link.SectionAlignment
['R_1', 'R_2']