Main window

This is the start-up window that opens when CS+ is launched.

In this window, you can control the user program execution and open panels.

Figure A-1. Main Window



The following items are explained here.

- [How to open]

- [Description of each area]

[How to open]

- Select Windows [Start] >> [Programs] >> [Renesas Electronics CS+] >> [CS+].

[Description of each area]

(1) Menu bar

This displays menus about real-time OS package.

(a) [View]

Realtime OS

Displays a cascading menu for relating to real-time OS package.

Resource Information

Opens the Realtime OS Resource Information panel.

Program Analyzer

Program analyzer is started.

[RI850V4 V1.xx.xx]

Opens the AZ850V4 window.

[RI78V4 V1.xx.xx]

Opens the AZ78K0R window.

Task Analyzer 1

Opens the Realtime OS Task Analyzer 1 panel.

[RI78V4 V2.xx.xx][RI850V4 V2.xx.xx][RI600V4]

Task Analyzer 2

Opens the Realtime OS Task Analyzer 2 panel.

[RI78V4 V2.xx.xx][RI850V4 V2.xx.xx][RI600V4]



(2) Toolbar

The toolbar shows command buttons relating to real-time OS package.

Opens the Realtime OS Resource Information panel.

Opens the Realtime OS Task Analyzer 1 panel. [RI78V4 V2.xx.xx]

[RI850V4 V2.xx.xx][RI600V4]

Opens the Realtime OS Task Analyzer 2 panel. [RI78V4 V2.xx.xx]

[RI850V4 V2.xx.xx][RI600V4]



(3) Panel display area

Panels are displayed in this area.