A.1 Description

Below is a list of the windows related to tools offered in the real-time OS package.

Table A-1. Window/Panel/Dialog Box List

Window/Panel/Dialog Box Name

Function Description

The first window opened when CS+ starts.

Create Project dialog box

Creates a new project or subproject.

(See "CS+ Start" for details.)

Project Tree panel

Displays the project elements as a tree.

(See "RI78V4 V2.xx.xx/RI850V4 V2.xx.xx/RI600V4/RI600PX/RI850V4/RI850MP/RI78V4 Coding" for details.)

Property panel

Displays details and change the settings of the node selected in the Project Tree panel.

(See "RI78V4 V2.xx.xx/RI850V4 V2.xx.xx/RI600V4/RI600PX/RI850V4/RI850MP/RI78V4 Real-Time Operating System User's Manual: Coding" for details.)

Realtime OS Resource Information panel

Displays real-time OS resource information (system information, memory area information, etc.).

(See "RI78V4 V2.xx.xx/RI850V4 V2.xx.xx/RI600V4/RI600PX/RI850V4/RI850MP/RI78V4 Real-Time Operating System User's Manual: Debug" for details.)

Realtime OS Task Analyzer panel

[RI78V4 V2.xx.xx][RI850V4 V2.xx.xx]

[RI600V4]

Displays information required to analyze the processing program (the status of execution transition of programs being processed, usage of real-time OS resources, usage of the CPU, etc.).

(See "RI78V4 V2.xx.xx/RI850V4 V2.xx.xx/RI600V4 Real-Time Operating System User's Manual: Analysis" for details.)

Program analyzer window (AZ850V4 window) [RI850V4 V1.xx.xx]

Executes basic operation of program analyzer.

(See "RI850V4 Real-Time Operating System User's Manual: Analysis" for details.)

Program analyzer window (AZ78K0R window) [RI78V4 V1.xx.xx]

Executes basic operation of program analyzer.

(See "RI78V4 Real-Time Operating System User's Manual: Analysis" for details.)