Download and install page


This page displays a list of selected updates, and starts the download and installation process.

Figure A.3

Download and install Page

 

The following items are explained here.

[How to open]

-

From the CS+ Update Manager window menu area, click [Download and install].

-

From the Select updates page main area, click [Download and install].

[Description of each area]

(1)

Button [Install]

Begins the download and installation process.

This button is disabled if no updates are selected.

Caution

If an emulator USB driver is installed, the confirmation dialog box may appear.

(2)

Update Selection area

Displays a list of items to update.

The following information is displayed for each update.

Category

Displays the category of the update.

Updates with the same category are displayed together.

Title

Displays the title of the update.

Download size

Displays the download size of the update.

Summary

Displays a summary of the update information.

Detail

This appears if there is detailed information about the update. Selecting it will display details in a browser.