You can delete all the intermediate files and generated files output by running a build (hereafter referred to as "clean").
Running a clean is performed for the entire project (main project and subprojects) or active project (see "2.7.5 Change the build target project").
From the [Build] menu, select [Clean Project].
Select the project, and then select [Clean active project] from the context menu.