Renesas Electronics
top
Project Operation
FUNCTIONS
Change the Window Layout
2.10
Change the Window Layout
This section describes how to change the CS+ window layout.
Previous Topic
Close a project
Next Topic
Automatically hide panels
Table of Contents
Overview
Start CS+
Create a Project
Manipulate a Project
Change the Build Tool Version
Set Build Target Files
Make Settings for Build Operations
Run a Build
Save the Project File
Change the Window Layout
Automatically hide panels
Float a window
Dock windows
Display multiple panels
Reset the window layout
Accelerate the Startup Time of CS+
Manipulate CS+ on the Command Line