Starts RIIC slave transmission.
Remarks 1. | This API function repeats the byte-level RIIC slave transmission from the buffer specified in argument tx_buf the number of times specified in argument tx_num. |
Remarks 2. | When performing a RIIC slave transmission, R_RIICn_Start must be called before this API function is called. |
[Syntax]
#include "r_cg_macrodriver.h"
void R_RIICn_Slave_Send ( uint8_t * const tx_buf, uint16_t tx_num );
|
Remark | n is the channel number. |
[Argument(s)]
|
|
|
|
|
|
uint8_t * const tx_buf;
|
Pointer to a buffer storing the transmission data
|
|
|
uint16_t tx_num;
|
Total amount of data to send
|
[Return value]
None.