|
r_riicn_transmitend_interrupt
|
Performs processing in response to the transmit end interrupts (TEI).
Remark | This API function is called to run interrupt processing for the transmit end interrupts (TEI). |
[Syntax]
static void r_riicn_transmitend_interrupt ( void );
|
Remark | n is the channel number. |
[Argument(s)]
None.
[Return value]
None.