-
cre_mbx
acre_mbx
-
ER cre_mbx (ID mbxid, T_CMBX *pk_cmbx );
ER_ID acre_mbx ( T_CMBX *pk_cmbx );
|
|
|
|
|
|
ID mbxid;
|
ID number of the mailbox.
|
|
|
T_CMBX *pk_cmbx;
|
Pointer to the packet containing the mailbox creation information.
|
[Mailbox creation information packet : T_CMBX]
typedef struct t_cmbx {
ATR mbxatr; /*Mailbox attribute*/
PRI maxmpri; /*Maximum message priority*/
VP mprihd; /*For future expansion*/
} T_CMBX;
|
This service call can be called from tasks that belong to
Trusted Domain.
The cre_mbx creates a mailbox with mailbox ID indicated by
mbxid according to the content of
pk_cmbx. The acre_mbx creates a mailbox according to the content of
pk_cmbx, and returns the created mailbox ID.
1 ) Mailbox attribute (
mbxatr)
The following are specified for
mbxatr.
mbxatr := ( ( TA_TFIFO || TA_TPRI | ( TA_MFIFO || TA_MPRI ) )
-
TA_TFIFO ( = 0x0000)
Task wait queue is managed in FIFO order.
-
TA_TPRI ( = 0x0001)
Task wait queue is managed in task current priority order. Among tasks with the same priority, they are queued in FIFO order.
-
TA_MFIFO ( = 0x0000)
Message queue is managed in FIFO order.
-
TA_MPRI ( = 0x0002)
Message queue is managed in message priority order. Among messages with the same priority, they are queued in FIFO order.
2 ) Maximum message priority (
maxmpri)
When TA_MPRI is specified for
mbxatr, the range of message priority which can be used is from 1 to
maxmpri. Ranges of the value that can be specified are from 1 to
TMAX_MPRI.
3 )
mpdihd
The
mprihd is for future expansion, and is only disregarded.
|
|
|
|
|
|
|
Normal completion of acre_mbx. (Created mailbox ID)
|
|
|
|
Normal completion of cre_mbx.
|
|
|
|
- Either of bits in mbxatr except bit0 and bit1 is 1.
|
|
|
|
- When TA_MPRI is specified
|
|
|
|
Invalid ID number. (only for cre_mbx)
|
|
|
|
- This service call was issued in the CPU locked state.
- This service call was issued from non-task.
- This service call was issued in the status "PSW.IPL > kernel interrupt mask level".
|
|
|
|
- Stack pointer points out of user stack for invoking task.
- The operand-read access to the area indicated by pk_cmbx has not been permitted to the invoking task.
|
|
|
|
- The invoking task does not belong to trusted domain.
|
|
|
|
No ID number available.(only for acre_mbx)
|
|
|
|
Object state error. (only for cre_mbx)
- The mailbox specified by mbxid exists.
|