-   
 
 rcv_mbx
 
-   
 
 Receive from mailbox (waiting forever).
 
 ER      rcv_mbx (ID mbxid, T_MSG **ppk_msg);
 
| 
 | 
 | 
 | 
| 
 | 
 ID      mbxid;
 
 | 
 ID number of the mailbox.
  
 | 
| 
 | 
 T_MSG   **ppk_msg;
 
 | 
 Start address of the message packet received from the mailbox.
  
 | 
 
 [Message packet T_MSG for TA_MFIFO attribute ]
 
 
 typedef struct {
     VP      msghead;       /*RI600PX management area*/
 } T_MSG;
 
 | 
 
 [Message packet T_MSG_PRI for TA_MPRI attribute]
 
 
 typedef struct {
     T_MSG   msgque;        /*Message header*/
     PRI     msgpri;        /*Message priority*/
 } T_MSG_PRI;
 
 | 
 
 This service call receives a message from the mailbox specified by parameter 
mbxid, and stores its start address in the area specified by parameter 
ppk_msg.
 
 If no message could be received from the target mailbox (no messages were queued to the wait queue) when this service call is issued, this service call does not receive messages but queues the invoking task to the target mailbox wait queue and moves it from the RUNNING state to the WAITING state (message reception wait state).
 
 The receiving WAITING state for a mailbox is cancelled in the following cases.
 
 
 Receiving WAITING State for a Mailbox Cancel Operation
  
 | 
 | 
 A message was transmitted to the target mailbox as a result of issuing  snd_mbx.
  
 | 
 | 
 A message was transmitted to the target mailbox as a result of issuing  isnd_mbx.
  
 | 
 | 
 Forced release from waiting (accept  rel_wai while waiting).
  
 | 
 | 
 Forced release from waiting (accept  irel_wai while waiting).
  
 | 
 | 
 Forced release from waiting (accept  del_mbx while waiting).
  
 | 
 | 
 
 Note	 Invoking tasks are queued to the target mailbox wait queue in the order specified at creating the mailbox (FIFO order or current priority order).
 
 
| 
 | 
 | 
 | 
| 
 | 
 | 
 | 
| 
 | 
 | 
 | 
| 
 | 
 | 
 | 
| 
 | 
 | 
 -	 This service call was issued from a non-task.
  
 -	 This service call was issued in the CPU locked state.
  
 -	 This service call was issued in the dispatching disabled state.
  
 -	 This service call was issued in the status "PSW.IPL > kernel interrupt mask level".
  
 | 
| 
 | 
 | 
 -	 Stack pointer points out of user stack for invoking task.
  
 -	 The operand-write access to the area indicated by  ppk_msg has not been permitted to the invoking task.
  
 | 
| 
 | 
 | 
 -	 The mailbox specified by  mbxid does not exist.
  
 | 
| 
 | 
 | 
 Forced release from the WAITING state.
  
 | 
| 
 | 
 | 
 |