Pushes to stack area (single register).
Pushes the value of the register specified by the operand to the stack area.
| When the push instruction is executed, the assembler executes instruction expansion to generate two or more machine instructions. | 
| Instruction expansion is performed, and set via an add instruction. |