Pops from stack area (single register).
Pops the value of the register specified by the operand from the stack area.
| When the pop instruction is executed, the assembler executes instruction expansion to generate two or more machine instructions. | 
| Instruction expansion is performed, and set via an add instruction. |