3.2.1 Structure of Linkage List

Table 3-3 shows the structure and contents of the linkage list.

Table 3.2

Structure and Contents of Linkage List

No

Output Information

Contents

When -show OptionNote is Specified

When -show Option is not Specified

1

Option information

Option strings specified by a command line or subcommand

None

Output

2

Error information

Error messages

None

Output

3

Linkage map information

Section name, start/end addresses, size, and type

None

Output

When -show=relocation_attribute is specified, the relocation attribute is output.

-show=relocation_attribute

Not output

4

Symbol information

Static definition symbol name, address, size, and type in the order of address

When -show=reference is specified:

Symbol reference count and optimization information in addition to the above information

When -show=struct is specified, information on the structure and union members is output.

-show =symbol

-show =reference

Not output

Not output

5

Symbol deletion optimization information

Symbols deleted by optimization

-show =symbol

Not output

6

Cross-reference information

Symbol reference information

-show =xreference

Not output

7

Total section size

Total sizes of RAM, ROM, and program sections

-show=total_size

Not output

8

Vector information

Vector numbers and address information

-show=vector

Not output

9

CRC information

CRC calculation result and output addresses

None

Always output when the CRC option is specified

Note

The -show option is valid when the list option is specified.