Error messages are output. The following figure shows an example of error information output.
*** Error Information ***
** E0562310 (E) Undefined external symbol "strcmp" referred to in "test.obj" (1)
|
|
|
|
|
|
Outputs an error message.
|
Note | As the number for the alignment of code sections whose address is determined after linkage, when big endian is selected, a multiple of 4 is indicated regardless of the actual number for alignment at the time of compiling and assembling. |