In this tutorial, the Pin Configuration and Code Generating functions are used.
In the default setting of CS+, the Pin Configuration and Code Generating functions are not available.
Set the plug-in by following the below procedure.
|
Select [Plugi-n Setting] from the [Tool] menu. |


|
After configuring the settings as shown in the figure below, click [OK]. |


|
Select [Yes], then CS+ restarts. |