Let us rebuild the program after creating sample project, and download the load module to simulator.
|
Click [Rebuild Project] button, and then click [Download] button. |


|
Layouts of main display get changed. |
Now, the preparing for trying analysis features is finished.
|
Tip |
To use an analysis function, it's necessary to output information for analyses in a build tool.
Build after setting "Enable static analysis information" as "Yes." and "Enable dynamic analysis information" as "Yes." in a property of analysis tool.
The sample project is made setting of "Yes.".