| 
 [General - Debug] category 
 | 
Use this category to configure general setting relating to debugging.
Figure A.51  | Option Dialog Box ([General - Debug] Category)  | 
 
 
The following items are explained here.
[How to open]
-  | From the [Tool] menu, select [Options...].  | 
 
[Description of each area]
(1)  | [Observe downloaded load module files changing]  | 
 
| 
 | 
 
Monitors load module files downloaded to the debugging tool for changes.  When there is a change, a message dialog box confirming whether to execute the download is displayed. 
 | 
| 
 | 
 
Does not monitor load module files downloaded to the debugging tool for changes (default). 
 | 
 
(2)  | [Add source files automatically (for the "Debug Only" project only)]  | 
 
| 
 | 
 
In a debug-dedicated project, when downloading a load module file into the debug tool, source files are automatically added to the project tree (default). 
 | 
| 
 | 
 
In a debug-dedicated project, when downloading a load module file into the debug tool, source files are not automatically added to the project tree. 
 | 
 
Caution  | This function is only valid when a load module file has been added to the Download files node of the project tree. 
When a load module file has been added in the [Download File Settings] tab on the Property panel of the debug tool, source files are not added to the project tree.  | 
 
| 
 | 
 
Beeps when the execution of a user program is halted due to a break event (hardware or software break). 
 | 
| 
 | 
 
Does not beep when the execution of a user program is halted due to a break event (hardware or software break) (default). 
 | 
 
(4)  | [Save the value of SFRs and IORs added in the Watch 4 panel]  | 
 
| 
 | 
 
Saves also the states of SFRs and IORs registered in the Watch 4 panel when saving the state of the debug tool.  Note that only the value of SFRs and IORs which can be read or rewritten will be saved. 
 | 
| 
 | 
 
Does not save the states of SFRs and IORs registered in the Watch 4 panel when saving the state of the debug tool.  Note that only the value of SFRs and IORs which can be read or rewritten will be saved (default). 
 | 
 
Caution  | This feature can be used only when there is a valid license.  | 
 
(5)  | [Enable rewind feature]  | 
 
| 
 | 
 
Automatically accumulates the memory and register values just before the debug tool is executed. 
 | 
| 
 | 
 
Automatically accumulates the memory and register values just before the debug tool is executed (default). 
 | 
 
(a)  | [Maximum number of times of rewinding]  | 
 
Specify the upper limit for accumulation by the rewind feature.
Either enter a number between 1 and 100 directly via the keyboard, or specify a number via the 
 buttons.  The default is 50.
Note that clicking on the [OK] or [Apply] button while this item remains blank causes the tab setting to remain at the previously saved value.
Caution  | This feature can be used only when there is a valid license.  | 
 
(6)  | [Do not distinguish source files with the same file name by the relative path]  | 
 
| 
 | 
 
When a source file in a project is associated with a given address and is to be opened in a new panel or shown in front of an existing display if the file has already been displayed in a panel, the relative path to the file is not used. 
Selecting this check box may disable the following operations in some projects. 
-  | Displaying the current PC mark on the Editor panel  |  
  
-  | [Go To...] from the context menu on the Editor panel  |  
  
-  | Displaying the source text in the Mixed display mode on the Disassemble panel  |  
  
-  | [Jump to Source] from the context menu on the Disassemble panel  |  
  
  
Select this check box if you wish to designate source files by their filenames alone. 
 | 
| 
 | 
 
When a source file in a project is associated with a given address and is to be opened in a new panel or shown in front of an existing display if the file has already been displayed in a panel, the relative path to the file is used (default). 
 | 
 
Caution  | If you select this check box and there are multiple source files with the same name within a load module, you may not be able to select the correct files.  | 
 
| 
 
Initialize Settings 
 | 
 
Returns all currently displayed setting to their default values. 
 | 
 
[Function buttons]
| 
 | 
 | 
| 
 
Initialize All Settings 
 | 
 
Restores all settings on this dialog box to their default values. 
Note, however, that newly added items in the [General - External Tools] category will not be removed. 
 | 
| 
 
OK 
 | 
 
Applies all setting and closes this dialog box. 
 | 
| 
 
Cancel 
 | 
 
Ignores the setting and closes this dialog box. 
 | 
| 
 
Apply 
 | 
 
Applies all setting (does not close this dialog box). 
 | 
| 
 
Help 
 | 
 
Displays the help of this dialog box. 
 |