2.7 Set Hex Output Options

To set options for the hex output phase, select the Build tool node on the project tree and select the [Hex Output Options] tab on the Property panel.

You can set the various hex output options by setting the necessary properties in this tab.

Caution

This tab is not displayed for the library project.

Figure 2.57

Property Panel: [Hex Output Options] Tab

 

Remark

Often used options have been gathered under the [Frequently Used Options(for Hex Output)] category on the [Common Options] tab.