2.8 Set Create Library Options

To set options for the librarian, select the Build tool node on the project tree and select the [Create Library Options] tab on the Property panel.

You can set the various create library options by setting the necessary properties in this tab.

Caution

This tab is displayed for the library project.

Figure 2.65

Property Panel: [Create Library Options] Tab

 

Remark

Often used options have been gathered under the [Frequently Used Options(for Create Library)] category on the [Common Options] tab.