2.8.1 Set the output of a library file

Select the build tool node on the project tree and select the [Create Library Options] tab on the Property panel.

The setting to output a library file is made with the [Output File] category.

Figure 2.66

[Output File] Category

 

(1)

Set the output format

Select the format in the [Output file format] property.

You can select any of the formats below.

Format

Configuration

User libraries(-FOrm=Library=U)

Outputs a user library file.

System libraries(-FOrm=Library=S)

Outputs a system library file.

The system library file is linked after the user library file.

Select this item to create a library that is to be linked after the user library file.

Relocatable file(-FOrm=Relocate)

Outputs a relocatable file.

(2)

Set the output folder

Setting the output folder is made with the [Output folder] property by directly entering to the text box or by the [...] button.

Up to 247 characters can be specified in the text box.

This property supports the following placeholder.

 

%ActiveProjectDir%: Replaces with the absolute path of the active project folder.

%ActiveProjectName%: Replaces with the active project name.

%BuildModeName%: Replaces with the build mode name.

%MainProjectDir%: Replaces with the absolute path of the main project folder.

%MainProjectName%: Replaces with the main project name.

%MicomToolPath%: Replaces with the absolute path of the install folder of this product.

%ProjectDir%: Replaces with the absolute path of the project folder.

%ProjectName%: Replaces with the project name.

%TempDir%: Replaces with the absolute path of the temporary folder.

%WinDir%: Replaces with the absolute path of the Windows system folder.

 

"%BuildModeName%" is set by default.

(3)

Set the output file name

Setting the output file is made with the [Output file name] property by directly entering to the text box.

If the extension is omitted, it is automatically added according to the selection in the [Output file format] property.

 

When [User libraries(-FOrm=Library=U)] is selected: .lib

When [System libraries(-FOrm=Library=S)] is selected: .lib

When [Relocatable file(-FOrm=Relocate)] is selected: .rel

 

Up to 259 characters can be specified in the text box.

This property supports the following placeholders.

 

%ActiveProjectName%: Replaces with the active project name.

%MainProjectName%: Replaces with the main project name.

%ProjectName%: Replaces with the project name.

 

"%ProjectName%.lib" is set by default.