Renesas Electronics
R_TAUDn_Create_UserInit
Performs user-defined initialization relating to the timer array unit Dn.
Remark
This API functions is called as the R_TAUDn_Create callback routine.
[Syntax]
void R_TAUDn_Create_UserInit ( void );
Remark n is the unit number.
[Argument(s)]
None.
[Return value]