r_taudn_channelm_interrupt


Performs processing in response to the timer interrupt.

[Syntax]

void    r_taudn_channelm_interrupt ( void );

Remark n is the unit number, m is the channel number.

[Argument(s)]

None.

[Return value]

None.