r_cac_ferrf_interrupt


Performs processing in response to the frequency error interrupt.

Remark

This API function is called to run interrupt processing for the frequency error interrupt, which is generated when the clock frequency is not in the allowed range (from the minimum to the maximum value).

[Syntax]

static  void    r_cac_ferrf_interrupt ( void );

[Argument(s)]

None.

[Return value]

None.