r_cac_ovff_interrupt


Performs processing in response to the overflow interrupt.

Remark

This API function is called to run interrupt processing for the overflow interrupt, which is generated when the counter overflows.

[Syntax]

static  void    r_cac_ovff_interrupt ( void );

[Argument(s)]

None.

[Return value]

None.