Performs processing in response to the event link interrupt.
Remark | This API function is called to run interrupt processing for the event signal defined in event link setting register.
n is the source number.
|
[Syntax]
static void r_elc_elsrni_interrupt ( void );
|
Remark | n is the source number. |
[Argument(s)]
None.
[Return value]
None.