R_ELC_Get_PortBuffern


Gets the value of a port buffer.

[Syntax]

void    R_ELC_Get_PortBuffern ( uint8_t * const value );

Remark

n is the source number.

[Argument(s)]

I/O

Argument

Description

O

uint8_t * const value;

Pointer to the location where the obtained value is to be stored.

[Return value]

None.