| 
 r_mtu2_cj_tcivn_interrupt 
 | 
Performs processing in response to the overflow interrupt.
Remark  | This API function is called to run interrupt processing for the overflow interrupt, which is generated in response to an overflow of the timer counter (TCNT).  | 
 
[Syntax]
static  void    r_mtu2_cj_tcivn_interrupt ( void ); 
 | 
 
Remark  | j is the relationship channel number, and n is the channel number.  | 
 
[Argument(s)]
None.
[Return value]
None.