r_mtu2_tciun_interrupt


Performs processing in response to the underflow interrupt.

Remark

This API function is called to run interrupt processing for the underflow interrupt, which is generated in response to an underflow of the timer counter (TCNT).

[Syntax]

static  void    r_mtu2_tciun_interrupt ( void );

Remark

n is the channel number.

[Argument(s)]

None.

[Return value]

None.