R_RTC_Set_CalendarCounterValue
|
Sets the calendar and time values.
[Syntax]
#include "r_cg_rtc.h"
void R_RTC_Set_CalendarCounterValue ( rtc_calendarcounter_value_t counter_write_val );
|
[Argument(s)]
|
|
|
|
rtc_calendarcounter_value_t
counter_write_val;
|
Calendar and time values (year, month, date, day-of-week, time, minute, and second)
|
Remark | The configuration of the calendar and time values rtc_calendarcounter_value_t is shown below. |
typedef struct {
uint8_t rseccnt; /* second */
uint8_t rmincnt; /* Minute */
uint8_t rhrcnt; /* Time */
uint8_t rdaycnt; /* Date */
uint8_t rwkcnt; /* Day-of-week (0: Sunday, 6: Saturday) */
uint8_t rmoncnt; /* Month */
uint16_t ryrcnt; /* Year */
} rtc_calendarcounter_value_t;
|
[Return value]
None.