Performs processing in response to the transmit FIFO data empty interrupts.
Remark | This API function is called to run the interrupt processing for the transmit FIFO data empty interrupt. |
[Syntax]
static void r_scifan_txif_interrupt ( void );
|
Remark | n is the channel number. |
[Argument(s)]
None.
[Return value]
None.