r_scifan_erif_interrupt


Performs processing in response to the framing error or parity error interrupts.

Remark

This API function is called to run the interrupt processing for the framing error or parity error interrupt.

[Syntax]

static  void    r_scifan_erif_interrupt ( void );

Remark

n is the channel number.

[Argument(s)]

None.

[Return value]

None.