2.5.2 Change file name

In the Code Generator, select [Project name (Project)] >> [Code Generator (Design Tool)] >> [Code Preview] >> Peripheral function node >> Source code node in the Project Tree panel. The name of the file can be changed by selecting "Rename" from the context menu, which is displayed by right clicking the mouse.

Figure 2.9

Change File Name

 

Remark

To restore the default file name defined by the Code Generator, select [Default] from the context menu.