2.5.6 Change text file encodeing

The Code Generator is used to change the output destination folder for the source code by selecting [Code Generator Setting] tab >> [Generate File Mode] >> [Text file encoding] in the Property panel.

Figure 2.13

Change Output Destination Folder

Remark 'System' is set as the default setting.
When 'System' is selected, the encoding follows to Windows setting.