2.6 Output Report Files

Output report files (a file containing information configured using Code Generator and a file containing information regarding the source code) by first activating the Peripheral Functions panel or Code Preview panel, then selecting [File] menu >> [Save Code Generator Report].

The destination folder for the report file is specified by clicking [Code Generator Setting] tab >> [Generate File Mode] >> [Output folder] in the Property panel.

Figure 2.15

Output Example of Report File "Function" (HTML File)

 

Remark 1.

You can only use "Function" or "Macro" as a name of the report file.

See "2.6.1 Change output format" for details on the output format.

Function.xxx

A file that contains the information regarding the source code

Macro.xxx

A file that contains the information configured using Code Generator

Remark 2.

The output mode of the report file is defined in "Overwrite file".