slp_tsk

Outline

Put task to sleep (waiting forever).

C format

 ER      slp_tsk ( void );


Assembly format

 CALL    !!_slp_tsk


Parameter(s)

None.

Explanation

As a result, the invoking task is unlinked from the ready queue and excluded from the RI78V4 scheduling subject.

If a wakeup request has been queued to the target task (the wakeup request counter is not set to 0x0) when this service call is issued, this service call does not move the state but decrements the wakeup request counter (by subtracting 0x1 from the wakeup request counter).

Sleeping State Cancel Operation

Return Value

A wakeup request was issued as a result of issuing wup_tsk.

E_OK

A wakeup request was issued as a result of issuing iwup_tsk.

E_OK

Forced release from waiting (accept rel_wai while waiting).

E_RLWAI

Forced release from waiting (accept irel_wai while waiting).

E_RLWAI



Return value

Macro

Value

Description

E_OK

0

Normal completion.

E_RLWAI

-49

Forced release from waiting (accept rel_wai/irel_wai while waiting).