-
sus_tsk
isus_tsk
-
ER sus_tsk ( ID tskid );
ER isus_tsk ( ID tskid );
|
MOV A, #tskid
CALL !!_sus_tsk
MOV A, #tskid
CALL !!_isus_tsk
|
|
|
|
|
|
|
ID tskid;
|
ID number of the task to be suspended.
Value: ID number of the task to be suspended.
|
These service calls add 0x1 to the suspend request counter for the task specified by parameter
tskid, and then move the target task from the RUNNING state to the SUSPENDED state, from the READY state to the SUSPENDED state, or from the WAITING state to the WAITING-SUSPENDED state.
If the target task has moved to the SUSPENDED or WAITING-SUSPENDED state when this service call is issued, the counter manipulation processing is not performed but only the suspend request counter increment processing is executed.
SUSPENDED State Cancel Operation
|
|
A cancel request was issued as a result of issuing rsm_tsk.
|
|
A cancel request was issued as a result of issuing irsm_tsk.
|
|
Forced release from suspended (accept frsm_tsk while suspended).
|
|
Forced release from suspended (accept ifrsm_tsk while suspended).
|
|
Note 1 If the target task is the invoking task when this service call is issued, it is unlinked from the ready queue and excluded from the RI78V4 scheduling subject.
Note 2 The suspend request counter managed by the RI78V4 is configured in 7-bit widths. If the number of suspend requests exceeds the maximum count value 127 as a result of issuing this service call, the counter manipulation processing is therefore not performed but "E_QOVR" is returned.
|
|
|
|
|
|
|
|
|
|
|
Object state error (specified task is in the DORMANT state).
|
|
|
|
Queue overflow (overflow of suspension count "127").
|