-
act_tsk
iact_tsk
-
Activate task (queues an activation request).
ER act_tsk (ID tskid);
ER iact_tsk (ID tskid);
|
|
|
|
|
|
ID tskid;
|
ID number of the task to be activated.
Value: ID number of the task to be activated.
|
These service calls move a task specified by parameter
tskid from the DORMANT state to the READY state.
As a result, the target task is queued at the end on the ready queue corresponding to the initial priority and becomes subject to scheduling by the RI850V4.
If the target task has been moved to a state other than the DORMANT state when this service call is issued, this service call does not move the state but increments the activation request counter (by added 0x1 to the wakeup request counter).
Note 1 The activation request counter managed by the RI850V4 is configured in 7-bit widths. If the number of activation requests exceeds the maximum count value 127 as a result of issuing this service call, the counter manipulation processing is therefore not performed but "E_QOVR" is returned.
Note 2 Extended information specified in
Task information is passed to the task activated by issuing these service calls.
|
|
|
|
|
|
|
|
|
|
|
- tskid > Maximum ID number
- When this service call was issued from a non-task, TSK_SELF was specified tskid.
|
|
|
|
- This service call was issued in the CPU locked state.
|
|
|
|
- Specified task is not registered.
|
|
|
|
- Activation request count exceeded 127.
|