-
ter_tsk
-
ER ter_tsk (ID tskid);
|
|
|
|
|
|
ID tskid;
|
ID number of the task to be terminated.
|
This service call forcibly moves a task specified by parameter
tskid to the DORMANT state.
As a result, the target task is excluded from the RI850V4 scheduling subject.
If an activation request has been queued to the target task (the activation request counter is not set to 0x0) when this service call is issued, this service call moves the task to the DORMANT state, decrements the wakeup request counter (by subtracting 0x1 from the wakeup request counter), and then moves the task from the DORMANT state to the READY state.
Note When moving a task to the DORMANT state, this service call initializes the following information to values that are set during task creation.
If the target task has locked a mutex, the locked state is released at the same time (processing equivalent to
unl_mtx).
|
|
|
|
|
|
|
|
|
|
|
- tskid > Maximum ID number
|
|
|
|
- This service call was issued from a non-task.
- This service call was issued in the CPU locked state.
|
|
|
|
Illegal service call use.
- Specified task is an invoking task.
|
|
|
|
- Specified task is in the DORMANT state.
|
|
|
|
- Specified task is not registered.
|